Depending on the time of day and the grid that you're on, it's very common to have peak energy rates much higher than the off peak rate.
In these cases, you can use the battery to charge at the lower rates and discharge at the higher rates, saving a significant amount of money.
And if you don't need to use that energy, you can trade it back to the grid when prices rise, unlocking a new revenue stream for your business.

Renewable energy can sometimes be unreliable – the sun doesn't always shine, and the wind doesn't always blow.
BESS-as-a-Service allows you to store excess energy from solar or wind generation and use it later, enhancing the quality, capacity and resilience of renewable supply, and reducing your reliance on carbon-heavy grid power.
It also helps lower carbon emissions by using cleaner energy during peak demand times, and by replacing fossil fuel generators with clean backup power.
You can meet sustainability and ESG goals through improved energy efficiency by reducing emissions and supporting renewable energy use. Businesses can showcase their commitment to sustainability and track progress through data from the included energy management platform.
For businesses that require 100% uptime from their infrastructure, including their electrical assets, back-up power is a must. But in the past, this often meant expensive, carbon-intensive diesel-powered generators.
With BESS-as-a-Service from ABB, you can use clean, renewable energy to augment your back-up power. It's a great way to showcase your commitment to sustainability, and with the included energy management platform, you can track usage for ESG reporting.
ABB Electrification Service’s unique as-a-service model means that you can power your possibilities, thanks to a BESS solution, with no upfront capital expenditure. All the hardware, software, and support services are included in the as-a-service package.
We take care of the design of the system, the installation and commissioning including capital works, and even the ongoing maintenance of the system.
To find out more, request an obligation-free feasibility assessment.
The manufacturing sector is one of the most energy-intensive industries globally, making efficient energy management a critical priority. Rising energy costs, stricter environmental regulations, and the need for uninterrupted power are driving manufacturers to explore innovative solutions. Battery Energy Storage Systems (BESS) offer a transformative approach to achieve cost savings, improve sustainability, and ensure reliable power supply, says Andressa Ferraz, Sustainability Advisory Services Leader for the EMEA region.
The manufacturing sector is one of the most energy-intensive industries globally, making efficient energy management a critical priority. Rising energy costs, stricter environmental regulations, and the need for uninterrupted power are driving manufacturers to explore innovative solutions. Battery Energy Storage Systems (BESS) offer a transformative approach to achieve cost savings, improve sustainability, and ensure reliable power supply, says Andressa Ferraz, Sustainability Advisory Services Leader for the EMEA region.
When energy prices spike during high-demand periods, manufacturers feel the effect on their bottom line. With prices in certain markets rocketing by tens of thousands of percent, often for several hours, industry cannot afford to bear the cost.
A BESS allows facilities to store energy during off-peak times and deploy it during high-demand periods, minimizing demand charges and reducing operational costs. This practice not only reduces energy expenditure but also leads to more predictable and manageable operating costs, enhancing financial planning.
Additionally, BESS enables energy arbitrage, allowing manufacturers to purchase electricity during low-cost periods and feed it back to the grid when prices are higher. Unlocking a previously untapped revenue stream like this allows businesses to turn power into a profit line.
Many factories generate their own power – perhaps through solar cells or wind turbines. BESS allows these facilities to reduce their reliance on fossil fuels. By storing excess renewable energy, facilities can rely on clean power even during periods of low generation, reducing their carbon footprint and enabling them to take a giant step toward net zero operations.
Adopting a BESS also allows manufacturers to comply with stricter environmental regulations. Improved sustainability profiles boost brand reputation, align with consumer expectations, and attract eco-conscious investors.
Power outages and grid instability can severely disrupt manufacturing operations, leading to productivity losses and equipment damage. A BESS provides a reliable backup power source, ensuring continuous operations and minimizing costly downtime. And because batteries react faster than diesel generators – another source of pollution businesses are striving to avoid – downtime can be restricted to short interruptions, and perhaps eliminated completely.
Manufacturers don’t need to lose power completely to suffer from poor grid supply. Voltage fluctuations can negatively affect sensitive manufacturing equipment, leading to inefficiencies or breakdowns. A BESS helps improve power quality, smoothing out voltage fluctuations and enhancing the longevity and efficiency of machinery.
Battery Energy Storage Systems present a unique opportunity for the manufacturing sector to optimize costs, improve sustainability, and enhance power reliability. By embracing BESS, manufacturers can remain competitive, comply with environmental standards, and align with global trends toward cleaner energy.
But, while the long-term benefits of BESS are substantial, the upfront costs can be a hurdle, and seamlessly integrating BESS into existing manufacturing processes requires careful planning and expertise.
But with ABB’s unique BESS-as-a-Service model, all of those concerns can be put aside. Thanks to this model, implementing a BESS on your site is possible with no up-front capital expenditure. In addition, the planning, installation and ongoing maintenance of the equipment is handled by ABB – your single point of contact for all aspects of the implementation. You’ll also get access to management software that allows you to monitor the system from a single screen. And thanks to the savings possible with energy management, many of our customers see a positive financial return from day one.
Book an obligation-free feasibility assessment

A battery energy storage system, or BESS, is an onsite solution for energy storage. You can use the battery to store energy purchased from the grid, or energy that you have generated on your own premises. This energy can then be used to smooth out unreliable grid supply, bolster inadequate supply, or act as back-up in the event of total grid failure.
As well as being used for electricity storage, a BESS allows you to engage in energy arbitrage and peak shaving to make the most out of your energy use, and turn power into profit.
Precise battery capacity and chemistry is determined by customer need – ABB will work with you to determine your requirements and deliver a BESS solution that will help you meet all your objectives.
Energy arbitrage is the practice of purchasing energy when it is cheap, and selling it back to the grid when the prices are higher.
Businesses that generate their own energy, through solar panels or wind turbines for example, can also choose to sell excess energy back to the grid.
The most efficient way of generating income from energy arbitrage is to use automated software that tracks prices and capacity and programmatically trades energy when the rewards are largest.
Peak shaving is the practice of purchasing energy when rates are low – at night, for example – and storing it in a battery for use when the prices are higher.
The practice empowers businesses to optimise their energy use and reduce their overall operation costs.
The supply of power from electrical grids can sometimes be unreliable, especially when that power is provided via renewable methods. Power smoothing, or grid smoothing, is a practice that uses battery energy storage systems (BESS) to mitigate the problems of variable outputs from the grid.
BESS systems sit between your grid connection and the consumption of power, and use stored energy to smooth out the differences in output so that your equipment receives an uninterrupted, reliable energy supply.
The specifications of the battery you use will be defined by your need. ABB's BESS-as-a-Service solution includes a comprehensive analysis of your business objectives, energy use, and future expansion plans.
ABB guarantees that the useable capacity of your battery will meet your requirements for the life of the battery – even taking into account the natural degradation of battery capacity over time. That means if you need 5MW for 10 years, your battery will be designed to deliver that capacity for the whole life of the system.
ABB's BESS-as-a-Service uses a unique financing model that means there is no up-front capital expenditure required. Instead, the system is paid for using a predictable subscription plan, allowing you to build it into your ongoing operational expenditure.
You can find out more about the financing model in our guide for finance teams.
To find out more about ABB's BESS-as-a-Service offer, and how it can help you take control of energy, request an obligation-free feasibility assessment.